Our Challenge
AI for Disease Prevention
Research and development of a risk monitoring technology

Our Challenge
AI for Disease Prevention
Research and development of a risk monitoring technology
Preventing disease with self-monitored health data
Providing wellness to people is under the scope of OMRON Healthcare
When people and society talk about "wellness", what do they really mean? They want their families and friends to live each day with peace of mind, without feeling threatened by illness. As we move closer to our goal of Zero Events*, OMRON Healthcare will take up the challenge of preventing cerebrovascular and cardiovascular diseases using health data monitored at home.
*Zero Events: Reducing the incidence of cerebrovascular and cardiovascular diseases caused by high blood pressure to zero.
AI technology to explore possibilities presented by self-monitored health data
OMRON Healthcare cooperates with Kyoto University to leverage AI technology in fighting against hypertension.
OMRON Healthcare aims to make the best use of artificial intelligence technology to fully utilize blood pressure and other vital signs data monitored at home to health and prevent disease from developing and progressing.
To achieve this, OMRON Healthcare partnered with Kyoto University in a research project called “Healthcare AI Workshop.” Launched on June 1, 2021, the project aims to develop AI technology that can be used in an unprecedented way to enable effective control of hypertensive patients’ blood pressure and minimize risk for cerebrovascular and cardiovascular diseases.
The workshop strives to get the most out of health data monitored at home in order to prevent the incidence of serious disease as a part of daily living, and will focus on two themes to promote research.

Research theme #1: Creating a personalized blood pressure management method using AI
Of hypertensive patients undergoing treatment, 30% don’t control their blood pressure properly, according to 2019 guidelines from the Japanese Society of Hypertension.

Above data is retrieved from the National Health and Nutrition Survey in 2016. Population is retrieved from the demographic data in 2017.
Personalized blood pressure control enabled by AI technology.
This workshop aims to develop AI that can derive a blood pressure control method customized for each patient based on vital signs data monitored at home and lifestyle data, such as cigarette smoking and alcohol consumption.
Blood pressure fluctuates constantly throughout the day. Numerous factors cause these changes, including meals, exercise, sleep, stress, ambient temperature, and the pattern of changes also vary from person to person. OMRON Healthcare offers a wearable blood pressure monitor enabling measurement anytime during the day as well as a nocturnal monitor. These devices can be used to detect blood pressure fluctuations in the course of a normal day, and AI is used to discover the causal factors for these changes. This will facilitate medication planning and lifestyle improvement programs optimized for individuals. Once it becomes possible to customize blood pressure control for individual patients, patient motivation to seek treatment will also increase, and the burden on physicians can be reduced.
Research theme #2: Early detection of cerebrovascular/cardiovascular events making use of self-monitored health data using AI
Even if a patient controls blood pressure appropriately, it is impossible to completely eliminate the onset of serious events such as strokes or heart attacks. Enabling early-stage detection for such events is a key health challenge. Simply controlling blood pressure is not enough to reduce the incidence of cerebrovascular/cardiovascular diseases to zero. Because of this limitation, the research workshop will work to develop AI technology capable of detecting warning signs for these life-threatening events based on the blood pressure readings, ECG data, and other monitoring that patients can perform on a daily basis.
Enjoying better health and greater security every day with blood pressure control
The goal is to create an environment in which hypertensive patients will receive fully personalized healthcare on a timely basis, making the best use of health data that patients measure at home. This will help eliminate concerns regarding strokes or heart attacks, and enable patients to lead healthy lives with effective blood pressure control. And as we continue to advance our consultation support service, we also seek to reduce the burden borne by medical professionals, which is a critical social challenge today.


Our Journey

Our Challenge
Remote patient monitoring (RPM) service
Global RPM services aiming for zero cardiovascular diseasesAI for disease prevention
AI technology will be one of the future solutions to prevent cardiovascular diseasesEvolution of blood pressure management
Innovative devices and services for detecting hypertensionHeart Health
To detect atrial fibrillation (AF) at an early stage, new devices and services have been developedThank you for subscribing!